Setting Heap and Stack sizes for MK22

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Setting Heap and Stack sizes for MK22

2,761 次查看
Solarhacker
Contributor II

Using MCUXpresso IDE v11.2.1 with SDK_2.8.2_MK22FN128xxx12, Redlib (none)

Trying to change stack and heap size from default.  When I click on Heap or Stack Size (Default) No dialog is displayed.  I've tried --defsym=_HeapSize=0x0100 --defsym=_StackSize=0x0200 in linker flags

My project doesn't use any heap and stack requirements are less the 512 bytes. Currently out of 24K of RAM 7.5K are being consumed by unused heap and stack

>Darren

Solarhacker_0-1612816931144.png

 

0 项奖励
回复
3 回复数

2,730 次查看
Solarhacker
Contributor II

I finally got it to work. When I click on "default" stack size, nothing changes on display. if I enter a value and then left click again, value updates. Not expected dialog behavior.

0 项奖励
回复

2,744 次查看
ErichStyger
Specialist I

You can change the value from the default:

ErichS_0-1612867511971.png

 

Click into the field and enter a value.

 

I hope this helps,

Erich

2,749 次查看
frank_m
Senior Contributor III

Have you tried to enter approriate size values in the shown "Settings" screen, instead of leaving it at "Default" ?

There appears no additional screen for me, but I can manually enter values.

Version 11.1. for a LPC546xx, though.