Set PROGRAM_FLASH value in the IDE settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Set PROGRAM_FLASH value in the IDE settings

ソリューションへジャンプ
3,204件の閲覧回数
joao_ribeiro
Contributor IV

Hi,

We have a project where we would like to have the opportunity to compile it for using a bootloader version and compile it for a version without bootloader. For that I am using the compile in debug mode or in release mode, changing the code accordingly with #if DEBUG and #endif . But to totally accomplish it, we would like to change the PROGRAM_FLASH as well , setting it to 0xf000 for the bootloader and 0 for the debug version .

I am trying to find a way to do so but the MCUxpresso Properties->MCU settings are not defined by the compile mode, therefore I always have to change the PROGRAM_FLASH address every time I want to change the mode.

Is there a way to link the address to the compile mode so that the transition is just linked with the compilation mode?

Thank you for the help

Regards 

0 件の賞賛
返信
1 解決策
3,186件の閲覧回数
ErichStyger
Specialist I

See my article on this topic at https://mcuoneclipse.com/2019/10/06/linking-bootloader-applications-with-eclipse-and-freemarker-scri...

As you noted, the memory map/MCU settings do not support build configurations. I have filed a feature request on this, so I hope this could be available in a future version. Until then, the above approach with freemarker scripts works very well for me: I can build the booloader app or the standalone app. As long as the device stays the same with its overall memory map. Which is usually the case.

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,187件の閲覧回数
ErichStyger
Specialist I

See my article on this topic at https://mcuoneclipse.com/2019/10/06/linking-bootloader-applications-with-eclipse-and-freemarker-scri...

As you noted, the memory map/MCU settings do not support build configurations. I have filed a feature request on this, so I hope this could be available in a future version. Until then, the above approach with freemarker scripts works very well for me: I can build the booloader app or the standalone app. As long as the device stays the same with its overall memory map. Which is usually the case.

I hope this helps,

Erich

0 件の賞賛
返信
3,166件の閲覧回数
joao_ribeiro
Contributor IV

Hi @ErichStyger  ,

Thank you very much for the reply and help.

I am glad to hear that you have already filed a feature request on this , so I look forward to see it implemented on the next versions of the MCUxpresso, as it would help a lot.

Thank you also for the link on a way to work around this issue. I will try to implement it for sure.

Regards

0 件の賞賛
返信