SWO Not working under Linux (Ubuntu)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SWO Not working under Linux (Ubuntu)

1,624件の閲覧回数
alexandrekral
Contributor II

Product: MCUXpresso IDE
Version: MCUXpresso IDE v11.2.0 [Build 4120] [2020-07-09]
Operating system: Linux
VM: Java HotSpot(TM) 64-Bit Server VM (64 bit)

 

Everything is working fine in the debugger except for the SWO functions (SWO profile, ...).

The same exact config and code has been tested on a Windows 10 computer and the SWO Profile works perfectly well.

What could be wrong on Linux so that this particular functionality of the debugger doesn't work?

Is there anything to try and install?

Thank you.

0 件の賞賛
返信
1 返信

1,580件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Alexandrekral:

The SWO functionality depends on the target device. which device you are using?

The SWO also depends on the probe connection too. Only the most recent P&E debug probes do support SWO.

 

Regards

Daniel

0 件の賞賛
返信