SDK component replacement options will be ignored

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK component replacement options will be ignored

ソリューションへジャンプ
5,523件の閲覧回数
yo_ku_
Contributor II

I am using MCUXpressoIDE: v11.3.0 and have made modifications to the SDK component code (drivers, etc.).
When I refresh/add/remove SDK component in the project's SDK Management, the modification is detected and I can select Replace, Keep existing, or Compare.
But no matter which I select, the target file will be replaced.

Is there a plan to fix it?

SDK Management.png

 

Options.png

 

0 件の賞賛
返信
1 解決策
5,440件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

This is a IDE issue. It will be fixed in MCUX_IDE_v11.4.0.

Hope this helps,

Jun Zhang

元の投稿で解決策を見る

タグ(1)
6 返答(返信)
4,237件の閲覧回数
PhilV
Contributor III

Unless I'm missing something this is "fixed" in 11.9 by getting rid of the option completely?

Now when I update to a new SDK it replaces everything (no option of what to replace or not) and then I have to use my source control to show me what has changed and revert / edit any changes as necessary.

0 件の賞賛
返信
4,201件の閲覧回数
AdrianOltean
NXP Employee
NXP Employee

Would you please double-check the Preferences page which exposes the preferences that allows control of "Refresh SDK Components" behavior? Maybe you decided to keep/replace files at some point and also ticked "Remember my decision"?

AdrianOltean_0-1711537244274.png

Regards,

Adrian

 

0 件の賞賛
返信
5,441件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

This is a IDE issue. It will be fixed in MCUX_IDE_v11.4.0.

Hope this helps,

Jun Zhang

タグ(1)
5,427件の閲覧回数
yo_ku_
Contributor II

good news!

thanks!

0 件の賞賛
返信
5,497件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

I reproduce this issue. I will check it internally and will keep you informed.

 

Thanks,

Jun Zhang

0 件の賞賛
返信
5,452件の閲覧回数
Microfelix
Contributor IV

i have the exact same problem.

If I try to refresh the sdk and choose not to update, it will update itself

MCUXpresso IDE v11.3.1 [Build 5262] [2021-04-02]

 

Maurizio

0 件の賞賛
返信