Project has no MCUsetting,plesse install SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Project has no MCUsetting,plesse install SDK

1,548 Views
MERLIN_C
Contributor I

Hello, I'd like to inquire about the reason behind the following situation with MCUXpresso IDE: Every time I restart the debugger, it encounters the following issue (debugging works fine before restarting the IDE or the computer). How can I resolve this problem and ensure that the SDK doesn't need to be reinstalled after a reboot?

A.png

Thank you

 AAC

0 Kudos
Reply
1 Reply

1,525 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Can you confirm that the SDK is not deleted by some other process from the common SDK installation directory? Is your home folder cleaned automatically after reboot?

lpcxpresso_supp_0-1695207857736.png

Also, is your SDK listed in Installed SDKs view after restarting IDE/PC?

Regards,

MCUXpresso IDE Support

 

0 Kudos
Reply