Project has no MCUsetting,plesse install SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Project has no MCUsetting,plesse install SDK

1,547件の閲覧回数
MERLIN_C
Contributor I

Hello, I'd like to inquire about the reason behind the following situation with MCUXpresso IDE: Every time I restart the debugger, it encounters the following issue (debugging works fine before restarting the IDE or the computer). How can I resolve this problem and ensure that the SDK doesn't need to be reinstalled after a reboot?

A.png

Thank you

 AAC

0 件の賞賛
返信
1 返信

1,524件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Can you confirm that the SDK is not deleted by some other process from the common SDK installation directory? Is your home folder cleaned automatically after reboot?

lpcxpresso_supp_0-1695207857736.png

Also, is your SDK listed in Installed SDKs view after restarting IDE/PC?

Regards,

MCUXpresso IDE Support

 

0 件の賞賛
返信