Programming firmware into LPC4320 of HackRF-One device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming firmware into LPC4320 of HackRF-One device

3,111件の閲覧回数
wellington_ali
Contributor II

Hello.

I am going to develop and program my own firmware into LPC4320FBD144 of HackRF-One device.

Btw, I can't program successfully into this CPU in MCUXpresso IDE.

I think it may be resulted from the fact that I have not proper LinkServer Flash Driver.

I am using LPC Link-2.

Of course, I could program my own firmware using the method that HackRF manual explained.

But, it is based on their specific tools which are independent on MCUXpresso IDE.

Please help me.

0 件の賞賛
返信
3 返答(返信)

3,101件の閲覧回数
wellington_ali
Contributor II

Hello, Pavel.

Thank you very much for your reply.

In fact, I tried with these libraries many times.

I bought LPCXpresso-4367 board, and I succeeded based on these libraries with this dev-kit.

But, I couldn't complete with LPC4320 board (using HackRF-One's ).

In this process, I thought this maybe resulted from the fact that LPC4320 has not its own flash memory and it must use external flash memory.

Because of this idea, I said about LinkServer Flash Driver.

What is my mistake ?

Best regards.

 

0 件の賞賛
返信

3,095件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately, we do not have support for that board I think should go to the vendor or page from that vendor. I suggest reviewing the schematic of the board from NXP and comparing it with the other and reviewing if you need to populate some jumper.

Best regards,
Pavel

0 件の賞賛
返信

3,105件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I suggest downloading the SDK in this link LPCOpen Software for LPC43XX | NXP Semiconductors.

If you need more information please let me know.
Best regards,
Pavel

0 件の賞賛
返信