Program flash LPC-LINK2 issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program flash LPC-LINK2 issue

1,824件の閲覧回数
dawidstysiak
Contributor I

I noticed that when I use 

crt_emu_cm_redlink -flash-load-exec  ...

some bytes in the last sector of flash LPC1115 are not correct.

When I use command 

crt_emu_cm_redlink -flash-load

all is fine.

0 件の賞賛
返信
2 返答(返信)

1,737件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Using which toolchain - the old LPCXpresso IDE, or the current MCUXpresso IDE? And which version? And if using LPCXpresso IDE, please try the current MCUXpresso IDE out.

I would suggest posting more details into the appropriate toolchain forum. 

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信

1,737件の閲覧回数
dawidstysiak
Contributor I

I use the LPCXpresso IDE - v8.2.0. I will try MCUXpresso IDE. Thanks!

0 件の賞賛
返信