[NO SUBJECT]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[NO SUBJECT]

1,390 Views
tholkapiyanv
Contributor II
0 Kudos
Reply
1 Reply

1,294 Views
marek-trmac
NXP Employee
NXP Employee

Hi V. Thol Kapiyan,

there are MCUXpresso Config Tools allowing to configure MK22F device. Just download the tool, create new configuration for FRDM-K22F board and go to Peripherals tool that allows to configure FTM peripheral in graphical mode. This can help you easily experiment with different setting. Then you can copy-paste generated code into your application.

MCUXpresso Config Tools are also integrated into MCUXpresso IDE. If you are using IDE, I'd recommend to start with hello_world example project and then enable Peripherals.

Hope this helps.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply