[NO SUBJECT]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[NO SUBJECT]

1,385件の閲覧回数
tholkapiyanv
Contributor II
0 件の賞賛
返信
1 返信

1,289件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi V. Thol Kapiyan,

there are MCUXpresso Config Tools allowing to configure MK22F device. Just download the tool, create new configuration for FRDM-K22F board and go to Peripherals tool that allows to configure FTM peripheral in graphical mode. This can help you easily experiment with different setting. Then you can copy-paste generated code into your application.

MCUXpresso Config Tools are also integrated into MCUXpresso IDE. If you are using IDE, I'd recommend to start with hello_world example project and then enable Peripherals.

Hope this helps.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信