MCUXpresso Pin Configuration not working with K10 SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Pin Configuration not working with K10 SDK

1,405 Views
jkirklin
Contributor I

I have been using MCUXpresso version 11.3.1 with an MK10DN512VMD10 processor with no issues at all and all the tools work as expected. I was setting up the development environment on a new system and installed the latest version of MCUXpresso (11.5.0) and after installing the SDK for the K10DN512 processor, it appears that the Pins Tool does not work (The Peripherals and Clocks tools both work as expected once they are enabled). After enabling the Pins tool there is no generated code and no functional groups associated with it and it will not let me route pins with the tool Is there a workaround I can use or am I currently stuck with using the older version of the IDE that supports the K10 SDK? Also, after some quick tests, this appears to be an issue in version 11.4/11.4.1 as well.

0 Kudos
Reply
1 Reply

1,397 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI jkirklin 

Please see MCUXpresso Supported Devices Table

https://community.nxp.com/t5/MCUXpresso-General-Knowledge/MCUXpresso-Supported-Devices-Table/ta-p/11...

Pin Configuration Tool is available for K10

Please download the latest MCUXpresso IDE v10.5.0 

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-i...

and latest SDK:

https://mcuxpresso.nxp.com/en/select

Have a nice day

Jun Zhang

 

0 Kudos
Reply