I recently reinstalled MCUXpresso and now when I attempt to debug a target, it is asking me to register the PE Micro plugin. When I enter my email address I get the error "Could not register, please check your Internet connection. HTTP Status: 302" (screenshot attached).
My internet is fine. I removed my antivirus software with the same result. I attempted to connected to my internet such that I was bypassing our company firewall, with the same result.
Any idea how to get past this?
-Josiah
已解决! 转到解答。
Hi @justusandjustic,
that registration is optional and has no effect (except removing that register dialog in the launch config). So you don't have to do it.
As for the problem: I think it is an issue in the P&E plugin version you are using. For example I did upgrade my MCUXpresso IDE 11.5.1 to the latest one with the menu Help > Check for updates.
Then upgraded to the latest version:
After that, I was able to successfully register with P&E.
I hope this helps,
Erich
Hi @justusandjustic,
that registration is optional and has no effect (except removing that register dialog in the launch config). So you don't have to do it.
As for the problem: I think it is an issue in the P&E plugin version you are using. For example I did upgrade my MCUXpresso IDE 11.5.1 to the latest one with the menu Help > Check for updates.
Then upgraded to the latest version:
After that, I was able to successfully register with P&E.
I hope this helps,
Erich
Hello Josiah,
Which version do you used? There is no register with newest version 11.5:
Download from:
And also, it seems IDE can also work even though ignore the register.
BR
Alice