MCUXpresso PEMicro Plugin "Could not register"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso PEMicro Plugin "Could not register"

ソリューションへジャンプ
1,750件の閲覧回数
justusandjustic
Contributor III

I recently reinstalled MCUXpresso and now when I attempt to debug a target, it is asking me to register the PE Micro plugin.  When I enter my email address I get the error "Could not register, please check your Internet connection. HTTP Status: 302" (screenshot attached).

My internet is fine.  I removed my antivirus software with the same result.  I attempted to connected to my internet such that I was bypassing our company firewall, with the same result.

Any idea how to get past this?

-Josiah

0 件の賞賛
返信
1 解決策
1,725件の閲覧回数
ErichStyger
Specialist I

Hi @justusandjustic,

that registration is optional and has no effect (except removing that register dialog in the launch config). So you don't have to do it.

As for the problem: I think it is an issue in the P&E plugin version you are using. For example I did upgrade my MCUXpresso IDE 11.5.1 to the latest one with the menu Help > Check for updates.

Then upgraded to the latest version:

ErichStyger_0-1657697638802.png

 

After that, I was able to successfully register with P&E.

 

I hope this helps,

Erich

元の投稿で解決策を見る

3 返答(返信)
1,726件の閲覧回数
ErichStyger
Specialist I

Hi @justusandjustic,

that registration is optional and has no effect (except removing that register dialog in the launch config). So you don't have to do it.

As for the problem: I think it is an issue in the P&E plugin version you are using. For example I did upgrade my MCUXpresso IDE 11.5.1 to the latest one with the menu Help > Check for updates.

Then upgraded to the latest version:

ErichStyger_0-1657697638802.png

 

After that, I was able to successfully register with P&E.

 

I hope this helps,

Erich

1,720件の閲覧回数
justusandjustic
Contributor III

I updated my plugin as you suggested and was able to register successfully.

Thanks, Erich! 

-Josiah 

0 件の賞賛
返信
1,731件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Josiah,

Which version do you used? There is no register with newest version 11.5:

Download from:

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-i...  

 

And also, it seems IDE can also work even though ignore the register.

 

BR

Alice

0 件の賞賛
返信