When I create a new project for the MKE02Z4, I get the Flash Config Support Enabled and the ResetISR errors with the code it generates. This wasn't a problem with previous versions and I don't know how to fix it.
The Manage linker script check box is checked.
Please help.
已解决! 转到解答。
Hello again @dporada ,
You can create a new startup file only clicking this button:
This button refresh the SDK components by default including the startup file.
Also, if you experience any issue, do not hesitate to let me know.
BR
Habib.
Habib,
After you said this, I tried making a project on Windows 11 and it worked. I originally made the project on a Macintosh. Apparently the problem is only the Mac version. Can you still help?
Don
Hello again @dporada ,
In order to support you better, could you please provide me the next information when you presented the error?
-Mac architecture (Intel or Apple silicon)
-SDK version.
Also, is this the only MCU that presented the error?
BR
Habib.
Habib,
Apple silicon and SKD 2.10.0.
I tried with an MKM35Z part with the same problem.
Whatever changed, I cannot even open one of my old projects with an older version of MCUXpresso. I get the same errors.
Don
Hello again @dporada,
I was able to replicate your message error when I removed the part of code that is shown below:
That is the FlashConfig of the project and in the case that does not set, the linker script will put the error.
Fortunately, the SDK examples already have this configuration. Could you please build these examples to corroborate if the issue is only in your own projects? This is in order to try an pinpoint if the issue is from your custom SW or not.
Additionally. Exist a specific reason to use the version of the SDK 2.10 instead of the version 2.15?
BR
Habib.
Habib,
Updating to version 2.15 allows me create and build a new project. I thought that the software checked for updated SDKs.
I still cannot open old projects. I found the code you are talking about in the startup folder of working projects, but the startup folder is empty on previous projects. Copying the file to an older project caused 45 errors, so this won't fix it. How do I generate this file on previous projects?
Don
Hello again @dporada ,
You can create a new startup file only clicking this button:
This button refresh the SDK components by default including the startup file.
Also, if you experience any issue, do not hesitate to let me know.
BR
Habib.
Hello again @dporada,
Sorry for taking a while to get back to you.
I made tests with the SDK (version 2.15) and MCUxpresso version 11.9.1, I did not find any issues recreating the startup file.
In order to support you better can you provide me the project that has the issues?
BR
Habib.
Habib,
You were correct. I had 4 different versions of SDKs installed for that part. I deleted all of them and installed the MKM35Z512xxx7 and the TWR-KM35Z75M and they both worked.
Thank you,
Don
Here's the errors if this helps:
Building target: MKE02Z4_Project.axf
Invoking: MCU Linker
arm-none-eabi-gcc -nostdlib -Xlinker -Map="MKE02Z4_Project.map" -Xlinker --gc-sections -Xlinker -print-memory-usage -Xlinker --sort-section=alignment -Xlinker --cref -mcpu=cortex-m0plus -mthumb -T MKE02Z4_Project_Debug.ld -o "MKE02Z4_Project.axf" ./source/MKE02Z4_Project.o ./source/semihost_hardfault.o ./drivers/fsl_common.o ./drivers/fsl_port.o ./board/board.o ./board/clock_config.o ./board/peripherals.o ./board/pin_mux.o
/Applications/MCUXpressoIDE_11.9.1_2170/ide/plugins/com.nxp.mcuxpresso.tools.macosx_11.9.1.202402080819/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld: Linker Flash Config Support Enabled, but no .FlashConfig section provided within application
Memory region Used Size Region Size %age Used
/Applications/MCUXpressoIDE_11.9.1_2170/ide/plugins/com.nxp.mcuxpresso.tools.macosx_11.9.1.202402080819/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld: warning: cannot find entry symbol ResetISR; defaulting to 00000000
collect2: error: ld returned 1 exit status
make[1]: *** [makefile:46: MKE02Z4_Project.axf] Error 1
PROGRAM_FLASH: 1 KB 32 KB 3.12%
make: *** [makefile:37: all] Error 2
SRAM: 512 B 4 KB 12.50%
"make -r -j9 all" terminated with exit code 2. Build might be incomplete.
08:22:37 Build Failed. 3 errors, 1 warnings. (took 171ms)
Hello @dporada ,
I made a new project (with default settings) in the SDK_2.15.000_MKE02Z64xxx4 and with SDK_2.15.000_FRDM-KE02Z40M, both with the latest version that is the 2.15, and neither was built with errors.
In order to support you better, could you please provide me the steps that you made for create a new project?
BR,
Habib.