MCUXpresso IDE stuck while loading

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE stuck while loading

5,988 Views
sandeepthota
Contributor I

IDE is stuck after selecting workspace. Changing to new workspace did not help.

0 Kudos
Reply
5 Replies

5,981 Views
ErichStyger
Specialist I

can you check/share the .log inside the .metadata of the workspace folder?

 

Other than that, can you add the option

-clean

to the command/shortcut launching the IDE?

0 Kudos
Reply

5,970 Views
sandeepthota
Contributor I

@ErichStygerPlease find the attached log file. Interestingly it is not updating the log file while starting. Last time the log was updated is with -clean option and I removed the clean and started again and no update on to file.

0 Kudos
Reply

5,966 Views
converse
Senior Contributor V

The log says "Unable to clean the storage area:". This implies that there may be another version of MCUXpresso already running. Have you tried rebooting and then running again?

0 Kudos
Reply

5,965 Views
sandeepthota
Contributor I

Yes I did several times and it didn't help. I even uninstalled and reinstalled software to see if it fixes but didn't help

0 Kudos
Reply

5,961 Views
converse
Senior Contributor V

A couple of things to check:

Do you (as the runner of the program) have write access to the workspace?

Have you got any anti malware software running (virus/firewall)? Could this be stopping it?

0 Kudos
Reply