MCUXPresso IDE v. 10 cannot see LinkServer debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXPresso IDE v. 10 cannot see LinkServer debugger

2,438 Views
andreamendo
Contributor I

Hi,

I have both LPCXpresso v7.5.0 and MCUXpresso IDE v10.0.2 installed on my Windows 7 machine;

while the same project (based on LPC1518 mcu) is compiling and debugging fine with Redlink Server debugger, MCUXpresso IDE can't see LinkServer: the "Connect to Link Server" dialog box shows no items in "List of attached probes". I tryed reinstalling the driver, but nothing changes.

Insted, on a Linux machine debugging with MCUXPresso v10 and LinkServer is working. 

Any suggestion?

Tags (1)
0 Kudos
Reply
1 Reply

1,696 Views
lpcxpresso_supp
NXP Employee
NXP Employee

In the first place, please read through - section 14.12, "Using and troubleshooting LPC-Link2" of the MCUXpresso IDE v10.0.2 User Guide. My suspicion is that you have VCOM driver issues, as described in section14.12.6, "LPC-Link2 failing to enumerate".

Regards,

MCUXpresso IDE Support

0 Kudos
Reply