Linker Error: No linker script

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Linker Error: No linker script

8,191 次查看
curtis_hendrix
Contributor I

I have a project that I've imported, and I can build from the command line using our own build script (posted below), but I cannot build from within MCUXpresso.  The error I get is:

Internal: No linker script for vendor=NXP proc=cortex-m0plus nature=0, project=<project name>

The build script is

SET TOOLCHAIN_PATH=C:\nxp\MCUXpressoIDE_10.3.1_2233\ide\tools\bin
SET IDE=C:\nxp\MCUXpressoIDE_10.3.1_2233\ide\mcuxpressoidec.exe

"%IDE%" -nosplash --launcher.suppressErrors -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "c:\workspace" -import %~dp0Working\<project folder>

"%IDE%" -nosplash --launcher.suppressErrors -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "c:\workspace" -cleanBuild <project folder>/Debug

0 项奖励
回复
14 回复数

8,027 次查看
soledad
NXP Employee
NXP Employee

Hi, 

Do you still need help? Is it possible to share the files to reproduce the issue? 

Regards 

Soledad

0 项奖励
回复

8,027 次查看
curtis_hendrix
Contributor I

Any help on this would be appreciated.

0 项奖励
回复

8,027 次查看
BlackNight
NXP Employee
NXP Employee

Does it work if you do it in 'interactive' mode (with the IDE GUI)?

And it would be helpful if you could share the files to reproduce this.

Erich

0 项奖励
回复

7,892 次查看
cjwood
Contributor I

I see a similar problem, and the problem doesn't exist when doing it from an interactive account.

I see that when triggered from the command line, by our build system, under a non-interactive account, the workspace is created and projects are imported, the build is kicked off and makefiles are auto-generated, and at the end the build fails during linker stage with: 

../arm-none-eabi/bin/ld.exe: cannot open linker script file *projectname*_Debug.ld: No such file or directory

Another observation: The project references are also ignored - only the named project is built. This also works when run from an interactive account.

0 项奖励
回复

7,093 次查看
ileonov
Contributor I
0 项奖励
回复

7,880 次查看
converse
Senior Contributor V

What is your command line?

0 项奖励
回复

7,868 次查看
cjwood
Contributor I

 

It is written in powershell:

$WorkspaceDir = "$PSScriptRoot\..\..\Workspaces\BuildScriptWS"
$ProjectsDir = "$PSScriptRoot\..\..\Projects"
$MCUInstallBaseDir = "C:\nxp\MCUXpressoIDE_11.3.1_5262"

echo "Creating workspace at $WorkspaceDir"
cmd /c "$MCUInstallBaseDir\ide\mcuxpressoidec.exe -nosplash --launcher.suppressErrors -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data ""$WorkspaceDir"" -import ""$ProjectsDir\MyProj"" -import ""$ProjectsDir\MyProj_Library"" -import ""$ProjectsDir\MyProj_Bootloader"" -import ""$ProjectsDir\MyProj_bsp"" 2>&1"
if ($LASTEXITCODE -ne 0) { $(throw "Failed to create workspace" ) }

echo "Building $BuildConfiguration Application"
cmd /c "$MCUInstallBaseDir\ide\mcuxpressoidec.exe -nosplash --launcher.suppressErrors -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data ""$WorkspaceDir"" -build MyProj/$BuildConfiguration 2>&1"
if ($LASTEXITCODE -ne 0) { $(throw "Failed to build Application" ) }

 

0 项奖励
回复

7,859 次查看
converse
Senior Contributor V

What is BuildConfiguration?

have you tries -cleanBuild (instead of -build)?

0 项奖励
回复

7,845 次查看
cjwood
Contributor I

My Apologies, $BuildConfiguration = "Debug"

I have now also tried with -cleanBuild. I have also written the equivalent in a batch script and I see the same result.

0 项奖励
回复

7,836 次查看
converse
Senior Contributor V

Can you share the output from the command? At least the linker command and the error messages. Also look to see if a linker script has been generated (anywhere?). I know this works for me, but I am not on the latest and greatest version of MCUXpresso.

0 项奖励
回复

7,822 次查看
cjwood
Contributor I

The command and output are shown here. When run off the back of a TFS build agent I can see that the makefiles are generated but the linker script is not. When I run the same script locally I see the makefiles and linker scripts are generated as expected.

arm-none-eabi-c++ -nostdlib -Xlinker -Map="MyProj.map" -Xlinker --gc-sections -Xlinker -print-memory-usage -Xlinker --sort-section=alignment -Xlinker --cref -mcpu=cortex-m7 -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -T MyProj_Debug.ld -o "MyProj.axf" ./xip/evkmimxrt1170_flexspi_nor_config.o ./xip/fsl_flexspi_nor_boot.o ./source/fpga.o ./source/main.o ./source/semihost_hardfault.o ./flexspi/flexspi_hyperbus_ops.o ./flexspi/flexspi_nor_flash_ops.o ./OpenRTOS/kernel_source/portable/MemMang/heap_2.o ./OpenRTOS/kernel_source/portable/GCC/ARM_CM4F/port.o ./OpenRTOS/kernel_source/croutine.o ./OpenRTOS/kernel_source/event_groups.o ./OpenRTOS/kernel_source/list.o ./OpenRTOS/kernel_source/queue.o ./OpenRTOS/kernel_source/stream_buffer.o ./OpenRTOS/kernel_source/tasks.o ./OpenRTOS/kernel_source/timers.o ./OpenRTOS/OpenRTOS_Trace/trcBase.o ./OpenRTOS/OpenRTOS_Trace/trcHardwarePort.o ./OpenRTOS/OpenRTOS_Trace/trcKernel.o ./OpenRTOS/OpenRTOS_Trace/trcKernelPort.o ./OpenRTOS/OpenRTOS_Trace/trcUser.o ./OpenRTOS/OpenRTOSAbstraction/CHookFunctions.o ./OpenRTOS/OpenRTOSAbstraction/CPPHookFunctions.o ./OpenRTOS/OpenRTOSAbstraction/VMutex.o ./OpenRTOS/OpenRTOSAbstraction/VRTOS.o ./OpenRTOS/OpenRTOSAbstraction/VSemaphore.o ./OpenRTOS/OpenRTOSAbstraction/VTask.o ./OpenRTOS/OpenRTOSAbstraction/VTick.o ./OpenRTOS/OpenRTOSAbstraction/vqueue.o ./HAL/FlashInterface.o ./HAL/HDLCHardware.o ./HAL/PowerSourceInterface.o ./HAL/Wdog.o ./HAL/WdogInterface.o ./HAL/codrv_can_flexcan.o ./HAL/codrv_canbittiming.o ./HAL/codrv_cpu.o ./HAL/codrv_error.o ./HAL/hal_exceptions.o ./HAL/hal_id.o ./HAL/hal_interrupts.o ./HAL/hal_led.o ./HAL/hal_timer.o ./HAL/hyperbus.o ./Builder/Coordinator.o ./Builder/ProdData.o -lMyProj_CANopen -lMyProj_bsp -lMyProj_Library
c:/nxp/mcuxpressoide_11.3.1_5262/ide/plugins/com.nxp.mcuxpresso.tools.win32_11.3.0.202008311133/tools/bin/../lib/gcc/arm-none-eabi/9.3.1/../../../../arm-none-eabi/bin/ld.exe: cannot open linker script file MyProj_Debug.ld: No such file or directory
0 项奖励
回复

7,812 次查看
converse
Senior Contributor V

If this problem only happens with TFS, then I suggest you look there for the problem. Maybe permissions? Maybe firewall? I don't know, just throwing out ideas.

0 项奖励
回复

7,804 次查看
cjwood
Contributor I

I appreciate the help so far. Another route I want to try is running the TFS build agent in interactive mode (an interactive Windows user account) rather than as a service. I suspect this issue is caused by running via a service. However, this is difficult to set up with our IT infrastructure so will take some time to achieve.

0 项奖励
回复

7,793 次查看
converse
Senior Contributor V

If it helps, we use Jenkins (on Mac, Windows and Linux) and have no problems.

0 项奖励
回复