LinkServer Flash Programmer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LinkServer Flash Programmer

5,369件の閲覧回数
ssinghal
Contributor II

Hey there,

I am currently using LPC-Link2 to flash my mcu (mkv31f). Since I have several to these mcu's to flash. I was looking for an alternative to doing it other than using mcu expresso IDE. I believe that the IDE has LinkServer Flash Programmer as a pluggin, is it possible to get the application separably installed on my computer and I can flash .asf files to mcu directly. Thanks.

4 返答(返信)

5,267件の閲覧回数
ssinghal
Contributor II

Thank you so much. It was really helpful. 

0 件の賞賛
返信

5,267件の閲覧回数
ssinghal
Contributor II

Hey,

Thanks for the reply. The link you provided helped me a lot. But I am again hitting a road block. I am getting error (Ed:05: File 'udaspshat_1.15.axf' load failure: Ef(11). No flash configured) when I try to flash my mcu with cmd line tool but the same axf file works with gui flash programmer. I looked at thread  Version 8 can't flash (no flash configured)... Could with v7.5, but its unclear what the error means in my case. 

 Note: I am using LPCxpresso LPC-Link2 Rev B (LPC-Link2 | NXP ) and trying to flash MKV31F mcu

Thanks for your help!failure-programmer.PNG

0 件の賞賛
返信

5,267件の閲覧回数
converse
Senior Contributor V

Where did you get that command line from? The command line (-pLPC4370 -vendor=NXP) is for programming an LPC4370.

If you have a working GUI Flash configuration, all you need to do is "Just copy flash command to clipboard" and the command line command will be in your clipboard.

EDIT: Also take a look at chapter 14 in the User Guide, where it describes the Command Preview which shows the exact command line and any setup you need to do, to run it.

5,267件の閲覧回数
converse
Senior Contributor V
0 件の賞賛
返信