LPC845: Error:Wire ack fault - target connected?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC845: Error:Wire ack fault - target connected?

6,518 次查看
farha
Contributor I

I am using LPC845 . From debugging and programming image using LPC-Link 2 debug probe. I have installed MCUxpresso IDE v11.5.1_7266 to connect with the board via LPC-Link 2.

I couldn't able to flash to board. I can see below the error every time.

[Started server]
[Connected on port 3025]
redlink> ProbeList
Index = 1
Manufacturer = NXP Semiconductors
Description = LPC-LINK2 CMSIS-DAP V5.361
Serial Number = C2FYEWGR
VID:PID = 1FC9:0090
Path = \\?\hid#vid_1fc9&pid_0090&mi_00#8&1ebe619d&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
redlink> ProbeStatus
Index = 1
Manufacturer = NXP Semiconductors
Description = LPC-LINK2 CMSIS-DAP V5.361
Serial Number = C2FYEWGR
VID:PID = 1FC9:0090
Path = \\?\hid#vid_1fc9&pid_0090&mi_00#8&1ebe619d&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
IsOpen = FALSE
WireInitialized = FALSE
WireProtocol = JTAG
CoresConfigured = FALSE
PacketSize = 1024
Reference Count = 0
HasSWV = FALSE
HasETM = FALSE
HasJTAG = TRUE
HasSWD = TRUE
Probe Type = CMSIS-DAP
Probe Reference Count = 0
redlink> ProbeList
Index = 1
Manufacturer = NXP Semiconductors
Description = LPC-LINK2 CMSIS-DAP V5.361
Serial Number = C2FYEWGR
VID:PID = 1FC9:0090
Path = \\?\hid#vid_1fc9&pid_0090&mi_00#8&1ebe619d&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
redlink> ProbeStatus
Index = 1
Manufacturer = NXP Semiconductors
Description = LPC-LINK2 CMSIS-DAP V5.361
Serial Number = C2FYEWGR
VID:PID = 1FC9:0090
Path = \\?\hid#vid_1fc9&pid_0090&mi_00#8&1ebe619d&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
IsOpen = FALSE
WireInitialized = FALSE
WireProtocol = JTAG
CoresConfigured = FALSE
PacketSize = 1024
Reference Count = 0
HasSWV = FALSE
HasETM = FALSE
HasJTAG = TRUE
HasSWD = TRUE
Probe Type = CMSIS-DAP
Probe Reference Count = 0
redlink> ProbeIsOpen 1
FALSE
redlink> ProbeOpenByIndex 1
Probe Handle 1 Open
redlink> WireIsConnected 1
FALSE
redlink> WireSwdConnect 1
Error: Wire Ack Fault - target connected?

 

 

 

0 项奖励
回复
8 回复数

5,210 次查看
brentsinger
Contributor I

Same error. Over two LPC55S69 boards... I'm at my wits end.

 

0 项奖励
回复

6,497 次查看
ErichStyger
Specialist I

I would check first the wire/connection: maybe you have it connected with wrong orientation?

Are you using your custom board or a LPC845-BRK board?

0 项奖励
回复

6,482 次查看
farha
Contributor I

I am using  custom board.

I have shared wire/connection.

kindly check attachment.

0 项奖励
回复

6,480 次查看
ErichStyger
Specialist I

I mean that you check the connection/soldering on your board.

0 项奖励
回复

6,476 次查看
farha
Contributor I

I have checked , it is ok.

 

0 项奖励
回复

6,465 次查看
ErichStyger
Specialist I

Have you tried another debug probe, e.g. a J-Link or P&E Multilink?

Check the Vddsense pin on the SWD header: does it have 3.3V or Vdd on it?

Are you able to debug other boards with your probe with the same MCU?

Have you tried deleting the .launch and recreated it?

Other than that: I wrote a checklist here:

https://mcuoneclipse.com/2014/11/03/debugging-failure-check-list-and-hints/

 

I hope this helps,

Erich

0 项奖励
回复

6,499 次查看
DanielRuvalcaba
NXP TechSupport
NXP TechSupport
0 项奖励
回复

6,497 次查看
farha
Contributor I

I tried this but I didn't get solution.

I am getting same error.

kindly help me.

0 项奖励
回复