LPC-Link 2 USB bounce causing problems with virtual machine

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC-Link 2 USB bounce causing problems with virtual machine

ソリューションへジャンプ
2,703件の閲覧回数
andrewlentvorsk
Contributor II

When I'm using the LPC-Link 2 with MCUXpresso, the board connects and disconnects USB in quick succession when the various programs install new firmware every time (MCUXpresso and FlashMagic, for example).  This causes issue if you are trying to run MCUXpresso in a virtual machine.

Is there a setting or technique where I can install a firmware onto the LPC-Link 2 and have it stick so that those USB disconnects/reconnects don't happen?

Thanks.

1 解決策
2,501件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Try programming the probe firmware into the flash of your LPC-Link2, rather than allowing the IDE to softload it. You can do this using LPCScrypt : http://www.nxp.com/LPCScrypt

For more background information, see:

https://community.nxp.com/message/630661 

Regards,

MCUXpresso IDE Support

元の投稿で解決策を見る

2 返答(返信)
2,501件の閲覧回数
andrewlentvorsk
Contributor II

Thanks.  That was exactly what I needed and now that the board doesn't bounce the USB, things are much more reliable.

0 件の賞賛
返信
2,502件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Try programming the probe firmware into the flash of your LPC-Link2, rather than allowing the IDE to softload it. You can do this using LPCScrypt : http://www.nxp.com/LPCScrypt

For more background information, see:

https://community.nxp.com/message/630661 

Regards,

MCUXpresso IDE Support