LPC-Link 2 USB bounce causing problems with virtual machine

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-Link 2 USB bounce causing problems with virtual machine

Jump to solution
2,724 Views
andrewlentvorsk
Contributor II

When I'm using the LPC-Link 2 with MCUXpresso, the board connects and disconnects USB in quick succession when the various programs install new firmware every time (MCUXpresso and FlashMagic, for example).  This causes issue if you are trying to run MCUXpresso in a virtual machine.

Is there a setting or technique where I can install a firmware onto the LPC-Link 2 and have it stick so that those USB disconnects/reconnects don't happen?

Thanks.

1 Solution
2,522 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Try programming the probe firmware into the flash of your LPC-Link2, rather than allowing the IDE to softload it. You can do this using LPCScrypt : http://www.nxp.com/LPCScrypt

For more background information, see:

https://community.nxp.com/message/630661 

Regards,

MCUXpresso IDE Support

View solution in original post

2 Replies
2,522 Views
andrewlentvorsk
Contributor II

Thanks.  That was exactly what I needed and now that the board doesn't bounce the USB, things are much more reliable.

0 Kudos
Reply
2,523 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Try programming the probe firmware into the flash of your LPC-Link2, rather than allowing the IDE to softload it. You can do this using LPCScrypt : http://www.nxp.com/LPCScrypt

For more background information, see:

https://community.nxp.com/message/630661 

Regards,

MCUXpresso IDE Support