Kinetis Motor Suite (KMS)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Motor Suite (KMS)

2,227件の閲覧回数
maurodiotti
Contributor I

Hi all

Do you know when there will be a KMS version for MCUXpresso?

Mauro.

0 件の賞賛
返信
3 返答(返信)

2,000件の閲覧回数
orhaan
Contributor I

How could i download KMS software. I can not find it both on internet and nxp internet sites.

0 件の賞賛
返信

2,057件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mauro,

I get the answer :

"

The MCUXpresso SDK and IDE, CLOCKS and PINS do not yet support Kinetis Motor Suite.  KMS requires Kinetis SDK 1.3 mainline with IDE to be either KDS3.2  or IAR.  The software desgin team has the port on their todo list but it is not yet scheduled.  The port would be from SDK 1.3 to SKD 2.x latest, which as you may know is a complete re-write of the code.

The NXP motor control reference projects are supported with MCUXpresso tools and SDK. So if you need to spin a motor try out the Motor Control Automated Tuner (MCAT) built into the Freemaster tool. 

 

We do think KMS will be supported this year 2017.

"

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,057件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mauro,

I asked the related development team , and will reply .ASAP when I get it .

BR

Alice

0 件の賞賛
返信