Kinetis Motor Suite (KMS)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis Motor Suite (KMS)

2,228 次查看
maurodiotti
Contributor I

Hi all

Do you know when there will be a KMS version for MCUXpresso?

Mauro.

0 项奖励
回复
3 回复数

2,001 次查看
orhaan
Contributor I

How could i download KMS software. I can not find it both on internet and nxp internet sites.

0 项奖励
回复

2,058 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mauro,

I get the answer :

"

The MCUXpresso SDK and IDE, CLOCKS and PINS do not yet support Kinetis Motor Suite.  KMS requires Kinetis SDK 1.3 mainline with IDE to be either KDS3.2  or IAR.  The software desgin team has the port on their todo list but it is not yet scheduled.  The port would be from SDK 1.3 to SKD 2.x latest, which as you may know is a complete re-write of the code.

The NXP motor control reference projects are supported with MCUXpresso tools and SDK. So if you need to spin a motor try out the Motor Control Automated Tuner (MCAT) built into the Freemaster tool. 

 

We do think KMS will be supported this year 2017.

"

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,058 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mauro,

I asked the related development team , and will reply .ASAP when I get it .

BR

Alice

0 项奖励
回复