Installed NXP serial driver does not function on windows 10 education though it does on windows 10 pro.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installed NXP serial driver does not function on windows 10 education though it does on windows 10 pro.

ソリューションへジャンプ
4,738件の閲覧回数
xanthurum
Contributor II

What i posted on the microsoft website:

No errors came up while installing NXP MCUexpresso, the IDE installs all necessary drivers to debug.

Installing the program as an administrator makes no difference.

I reinstalled the drivers while in disabled driver signature enforcement, no difference.

The OS on my laptop has just been reinstalled because of the problems with vivado ide.

Though that was not necessary!

Since the last windows update on my laptop I had also Xilinx Vivado 17.3 launch problems.

Though these have been solved and not because of a clean install!

https://forums.xilinx.com/t5/Installation-and-Licensing/Vivado-2017-3-launch-problems/td-p/804367

System desktop:


Image

System laptop:

Image

Device manager desktop:

Image

Device manager laptop:

Image

Devices and printers desktop:ImageImagePlease advise.

The answer from Microsoft:

Hi,

This can be due to compatibility of driver issues. Since you're using Windows 10 Education, it is possible that the driver is not being recognized by the system. To help you resolve the issue, we suggest downloading a generic driver and see if it will resolve the issue. You can also check the device manufacturer's website directly for drivers compatible to Windows 10 Education. However, if the issue still persists, we suggest contacting the device manufacturer directly to have further assistance regarding the drivers.

Let us know if you need further assistance.

Dear NXP, please advise.

 
 
0 件の賞賛
返信
1 解決策
4,308件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

What board do you actually have plugged into your laptop?

As detailed in the MCUXpresso IDE User Guide, I suspect that you simply need to install the mbed serial port driver : Windows serial configuration - Handbook | Mbed 

Regards,

MCUXpresso IDE Support

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,308件の閲覧回数
xanthurum
Contributor II

Problem is solved, thanks. :smileyhappy:

0 件の賞賛
返信
4,309件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

What board do you actually have plugged into your laptop?

As detailed in the MCUXpresso IDE User Guide, I suspect that you simply need to install the mbed serial port driver : Windows serial configuration - Handbook | Mbed 

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信