Install plugin from marketplace failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Install plugin from marketplace failed

Jump to solution
2,702 Views
dkh
NXP Employee
NXP Employee

Hello,

How can I get integrated function to install a plugin from the marketplace to work ?

I am using IDE 11.6.1 but tried 11.6.0 with same results

dkh_5-1668705999935.png

 

I go here:

dkh_3-1668705812757.png

Find the plugin I want and click "install"

dkh_4-1668705891595.png

 

I'm trying to install a plugin using the IDE from the market place and get this error:

dkh_0-1668705576489.png

 

I click OK and get this:

dkh_1-1668705627288.png

 

I click confirm and get this:

dkh_2-1668705704703.png

 

0 Kudos
Reply
1 Solution
2,689 Views
ErichStyger
Specialist I

It works for me, so to me there is no issue on the plugin/server side.

Maybe you are in a restrictive VPN network? I have seen reports that this can cause issues, as not the full network traffic seems to be routed through.

Or that the security settings on your machine somehow cause this, as starting from Oct 14th 22 all traffic on the marketplace is with https.

But you can get the plugin directly from there to:

https://marketplace.eclipse.org/content/bined-binaryhexadecimal-editor

or from

https://bined.exbin.org/eclipse-plugin/

 

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
3 Replies
2,690 Views
ErichStyger
Specialist I

It works for me, so to me there is no issue on the plugin/server side.

Maybe you are in a restrictive VPN network? I have seen reports that this can cause issues, as not the full network traffic seems to be routed through.

Or that the security settings on your machine somehow cause this, as starting from Oct 14th 22 all traffic on the marketplace is with https.

But you can get the plugin directly from there to:

https://marketplace.eclipse.org/content/bined-binaryhexadecimal-editor

or from

https://bined.exbin.org/eclipse-plugin/

 

I hope this helps,

Erich

0 Kudos
Reply
2,695 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi dkh 

I just tested marketplace on my side but I didn't see probelm:

ZhangJennie_0-1668756738027.png

 

I click on install, I get this window

ZhangJennie_1-1668756768537.png

 

I use MCUXpresso v11.6.1. I would suggest you change anohter network.

Have a nice day,

Jun Zhang

 

 

0 Kudos
Reply
2,686 Views
dkh
NXP Employee
NXP Employee

Thank you. I will assume this is network or security issue. This can be closed

0 Kudos
Reply