Implement MS OS descriptor functionality in virtual printer bm example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Implement MS OS descriptor functionality in virtual printer bm example

1,998件の閲覧回数
shabaka101694
Contributor I

Hello, 

 We are trying to use the virtual printer bm example specifically : lpcexpresso_54s018_dev_printer_virtual_plain_text_bm example. 

 

We have the basic functionality working, but need to add MS OS descriptor functionality so that the USB device registers as a WinUSB and therefore no driver signing is necessary. 

We are seeing Windows request the stringDescriptor at index 0xEE. We are having trouble getting Windows to request the other two needed descriptors. Specifically :

the WINUSB_ExtendedCompatId Descriptor

and

the WINUSB_ExtendedProperty_InterfaceGUID_Descriptor

 

Is it possible to provide some help/guidance on how we can get Windows to request these two descriptors using the previously mentioned example as a starting point 

 

Thanks 

Victor 

 

0 件の賞賛
返信
2 返答(返信)

1,902件の閲覧回数
Xu_Zhang
NXP Employee
NXP Employee

hi,shabaka101694

You can refer to this question and answer, hope it will help you.

https://community.nxp.com/t5/MCUXpresso-General/LPC54S018-WinUSB-driver-signing/td-p/1703179

BR

Xu Zhang

0 件の賞賛
返信

1,965件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Regarding the question about  MS OS descriptor functionality in virtual printer bm example, I have asked AE team, I will answer you after I get response.

BR

XiangJun Rong

0 件の賞賛
返信