How to setup MCUXpresso IDE for using QN9080-DK board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to setup MCUXpresso IDE for using QN9080-DK board

1,937件の閲覧回数
olivieradjemian
Contributor I

Hello,

I try to use QN9080-DK board, but it didn't appear into the "board and/or device selection page into IDE "New Project" section.

Thanks,

Olivier

0 件の賞賛
返信
2 返答(返信)

1,698件の閲覧回数
humberto_debrito
NXP Employee
NXP Employee

Hi Olivier,

As LPCX presso support said, you should download the SDK files from SDK Builder page (follow the link provided).

After that, you may find this tutorial interesting: MCUXpresso IDE - Importing SDK Example Project|NXP 

To install the SDK, you can simply drag and drop its .zip file into the "Installed SDKs" view tab.

Hope this answer is useful.

Best Regards,

Humberto.

0 件の賞賛
返信

1,698件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Hi Olivier,

QN9080 support is available to download in SDK format. Visit Welcome | MCUXpresso SDK Builder. You'll need to create a login if you don't already have one.

Thanks and regards,

MCUXpresso Support