How to import CMSIS-DSP examples?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to import CMSIS-DSP examples?

Jump to solution
5,235 Views
jerrylian
Contributor IV

Inside MCUXpresso-IDE:

* when we click "Import SDK examples", we see many examples but not DSP examples!

* I check folder: ........\SDK_2.2_TWR-K60D100M\CMSIS\DSP_Lib\Examples

--- I saw *.uvoptx/.uvprojx files

 

So, can we import DSP examples in MCUXpresso-IDE? or we need to use Keil uVision?

Thanks!

Jerry

0 Kudos
Reply
1 Solution
4,698 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jerry,

You can install Keil to run the DSP examples,

or if you want use MCUXpresso IDE, please refer to the below DOC to use CMSIS-DSP,

it introduce the steps on kds, while it is the same with MCUXpresso IDE.

Adding CMSIS-DSP Library to a KSDK 2.x project in Kinetis Design Studio 

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
4,699 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jerry,

You can install Keil to run the DSP examples,

or if you want use MCUXpresso IDE, please refer to the below DOC to use CMSIS-DSP,

it introduce the steps on kds, while it is the same with MCUXpresso IDE.

Adding CMSIS-DSP Library to a KSDK 2.x project in Kinetis Design Studio 

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
4,698 Views
jerrylian
Contributor IV

Hi Alice:

I followed your instructions:

* now I import DSP examples into MCUXpresso-IDE successfully.

* And it also solves my another problem of "hard fault".

Thanks a lot!

Jerry

0 Kudos
Reply