How to choose alternative cross gcc

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to choose alternative cross gcc

跳至解决方案
4,802 次查看
bastian_schick
Contributor IV

My problem: I cannot use the supplied arm-none-eabi-gcc. But I cannot see if and where I can point a project to my own GCC.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
4,688 次查看
bastian_schick
Contributor IV

Ok, possible (not best) solution: Change PATH in the project to point first to my gcc.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
4,689 次查看
bastian_schick
Contributor IV

Ok, possible (not best) solution: Change PATH in the project to point first to my gcc.

0 项奖励
回复
4,688 次查看
ErichStyger
Specialist I

or: swap the toolchain in C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\tools\arm-none-eabi

?

0 项奖励
回复
4,688 次查看
bastian_schick
Contributor IV

This is the worst idea. The same GCC is used also by Makefiles and IDEs other then Xpresso.

In TI's CCS it is easy to add another compiler (also Eclipse based).

So I consider it a "Bug" in Xpresso. ;-)

0 项奖励
回复
4,688 次查看
ErichStyger
Specialist I

No, this toolchain is used by MCUXpresso IDE (and only by that version), as it is inside the IDE installation folder. So you can replace that one. But of course it will be that toolchain for all your projects you are using with that installation folder. If you still want to use another one (or the original one), you can install yet another instance of the IDE.

If you want to set the toolchain for each project: you can use the GNU MCU (now part of Eclipse CDT) plugins: GNU MCU → Eclipse Embedded CDT! 

0 项奖励
回复
4,688 次查看
bastian_schick
Contributor IV

So, this renders MCUXpresso useless if the tool chain cannot be replaced. At least "any" GCC one should be possible.
Well, I can use the workaround. Still, I consider it a bug of MCUXpresso to be bound to "one" tool chain.

0 项奖励
回复