How to build 2 binaries in one shot for different memory configuration in mcuxpresso?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to build 2 binaries in one shot for different memory configuration in mcuxpresso?

1,459 Views
subbanna_manjun
Contributor I

Hi,

I have a requirement to build the application to 2 flash locations say 0x10000000 and 0x10032000.

I want to do it in one shot, by using pre and post build scripts. I am using mcuxpresso as IDE. So, if anyone could help on how to configure the scripts to change the program memory configuration during compile time it would be of great help.

Thanks in advance.

0 Kudos
Reply
2 Replies

1,378 Views
converse
Senior Contributor V

I don't think this is possible:

1. A project can only have one memory configuration. 2 memory configurations = 2 projects

2. Even if you could change memory configs (which you can't), you cannot build 2 targets in 1 build. 1 build = 1 target

Ideas on how you might make this a bit easier.

1. Set up two projects. Use linked resources (described in online Help) so they both use the exact same source.

 Or

2, (if the ONLY difference is the link step memory map), have 3 projects - one builds a library from your source, the other two have the separate memory configurations defined

0 Kudos
Reply

1,378 Views
ErichStyger
Specialist I

I'm doing it the following way:

Linking Bootloader Applications with Eclipse and FreeMarker Scripts | MCU on Eclipse 

I hope this helps,

Erich

0 Kudos
Reply