Gui Flash Tool - Repeat on completion, programs only two times

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gui Flash Tool - Repeat on completion, programs only two times

3,208 Views
wojtek327
Contributor I

Hello,

I am trying to program several boards using the GUI Flash Tool with MCU Link Pro. Programming LPC1769. I am using MCUXpresso IDE (MCUXpresso IDE v24.9 [Build 25] [2024-09-26]), and I have updated MCU Link Pro to the latest version. I checked the "Repeat on completion" flag. After clicking "Run," the tool successfully programs two boards, but on the third attempt, the programming process closes.

After clicking "Yes" to the prompt, "Do you want to perform the same operation again?" the programming stops, and I have to reopen the GUI Flash Tool. It seems like it can't reconnect with the probe after this. Is there any solution to this?

0 Kudos
Reply
2 Replies

3,183 Views
wojtek327
Contributor I

I worked around the problem by using the LinkServer software.

Tags (1)
0 Kudos
Reply

3,155 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @wojtek327 

 

Thanks for your sharing.

 

BR

Alice

0 Kudos
Reply