Fail to debug with LinkServer(Probe not open)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fail to debug with LinkServer(Probe not open)

7,325 Views
zzyzzy
Contributor I

Hi

I am a new for Mcuxpresso IDE.When I want to debug with LInkServer, I get a window which shows it can detect my device and probe. But when I continue, it comes a exception that probe not open and tells me that no connection to chips' debug port.How can I solve this debug problem?Thanks!

zzyzzy_0-1647074580121.pngzzyzzy_1-1647074593268.pngzzyzzy_2-1647074605551.pngzzyzzy_3-1647074614225.pngzzyzzy_4-1647074620510.png

 

regards

zzy

0 Kudos
Reply
9 Replies

7,225 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

Is your problem still happening? Are you using a custom board? Could you try to update the bootloader? 

Best regards,
Pavel

0 Kudos
Reply

7,217 Views
Bing
Contributor II

Yes, this is a custom board using MK66FN2M0VLQ18, and a MK20DX128VFM5 with OpenSDA v2.2 bootloader and DAPLink rev0244 firmware.

There are more than 80 students in the class, and for most of them the DAPLink debug probe works fine on their computer, but the problem mentioned above pops up on some computers persistently.

0 Kudos
Reply

7,221 Views
zzyzzy
Contributor I

Thanks for replying! The problem remains unsolved but closing all running programs and windows and restarting the computer with the board connecting can somehow solve this problem. I'm in quarantine so maybe I'll try your advice via my teacher's help after lifting the lockdown. Thanks again!

Best regards,

zzy

0 Kudos
Reply

7,192 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I recommend you try to get the newest version of MCUXpresso with the last one, refresh the openSDA with the last version. 

Best regards,

Pavel

0 Kudos
Reply

7,176 Views
Bing
Contributor II

Hi Pavel,

Actually we're all using the latest version of MCUXpresso IDE, v11.5.0 build 7232.

For OpenSDA bootloader and DAPLink firmware, we are using the latest version we can find, i.e. OpenSDA v2.2 and DAPLink rev0244. Or is there any newer version available?

Regards,

Bing

0 Kudos
Reply

7,158 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

I found some issues similar to this case. Could you please review the next threads? let me know if help you.

MCUXpresso Failing to discover CMISIS-DAP probe on... - NXP Community
Solved: Cannot start to debug session: MCUXpresso is stuck at... - NXP Community

Best regards,
Pavel 

0 Kudos
Reply

7,300 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI 

Please let us know your chip part number thus we can assign right engineer for your question.

Thanks,

Jun Zhang

0 Kudos
Reply

7,297 Views
zzyzzy
Contributor I

It is MK66FN2M0VLA18. Thanks!

0 Kudos
Reply

7,276 Views
Bing
Contributor II

It is MK66FN2M0VLQ18