FRDM-KL03Z Hello World Example, how-to make RX work?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KL03Z Hello World Example, how-to make RX work?

1,830件の閲覧回数
steffen_norbert
Contributor II

I need some help with the above mentioned example:

When used with semi-hosting the example works as expected. However when I use the UART, TX works as expected ("Hello world") while RX does not. I slightly changed the example from echoing to printing the hex value of the received character: Results are "consistent", i.e. the same char always produces the same hex value, however I can't find a meaningful pattern: sending  e.g. '1','2','3',... one would expect to see single bit or at most double bit changes, but  most of the time to many 1-Bits are produced. BTW: a loop-back test of my USB-serial-converter does work as expected.

If the problem is not known, some hints where to find (and read) configuration parameters and error flags would be greatly appreciated.

TX, Steffen

0 件の賞賛
返信
1 返信

1,708件の閲覧回数
steffen_norbert
Contributor II

I found the solution, when I read:

https://jaycarlson.net/pf/freescale-nxp-kinetis-kl03/ 

After removing C35 everything worked!

Other than mentioned in the FRDM-KL03 Users Guide, even 9600 Baud are too fast with C35 in place!

0 件の賞賛
返信