Error with OpenSDA connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error with OpenSDA connection

5,016 次查看
Flo2
Contributor I

Hello,

I'm using the AFBR-S50LV85D-EK evaluation kit with MCUXpresso IDE v11.9.0

I did a lot of test with this board, reprogramming it with the SDA connector.

But since this morning, I cannot reprogram it, I've got the message in attached.

Any idea to help me please ?

Thank you

0 项奖励
回复
8 回复数

4,860 次查看
Flo2
Contributor I

Hello Alice,

I don't have j-link debug probe. How can I proceed ?

Regards,

0 项奖励
回复

4,854 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Flo2 

Sorry maybe you misunderstood me. I mean update the firmware of OpenSDA to J-link. No external J-link debugger needed. 

Pay attention, if your system is win10. Please find a Win7 system PC to update.

Detail please refer to: 

https://www.nxp.com/design/design-center/software/sensor-toolbox/opensda-serial-and-debug-adapter:OP... 

Alice_Yang_0-1713347495564.png

 

BR

Alice

 

0 项奖励
回复

4,839 次查看
Flo2
Contributor I

@Alice_Yang,

What is the binary file I have to download ? OpenSDA V1 Bootloader ?

Where is the Segger JLink drivers in the download page?

Regards

 

0 项奖励
回复

4,754 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Flo2 

Steps as below:

1) Find a win7 PC.

2) Pressing RST button of your board, plug-in USB with SDA.

3) There should be a "bootloader" Drive on your PC.

4) Copy and paste the Application binary file into the BOOTLOADER drive. I attach the binary file to you.

5)Un-plug and re-plug the USB cable from the SDA USB port WITHOUT keeping reset button pressed.

 

BR

Alice

0 项奖励
回复

4,736 次查看
Flo2
Contributor I

Hello,

Will it works with a Windows 11 ?

Regards

0 项奖励
回复

4,684 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Flo2 

Update firmware need based on Win7 system.

After updated, board can work on Win11.

If you really no Win7, can try this method:

https://mcuoneclipse.com/2018/04/10/recovering-opensda-boards-with-windows-10/ 

 

BR

Alice

0 项奖励
回复

4,850 次查看
Flo2
Contributor I

@Alice_Yang ,

My PC is win11, could it works ?

标记 (1)
0 项奖励
回复

4,863 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Flo2 

How about updating debug firmware to j-link?

 

BR

Alice

0 项奖励
回复