Enabling Flash Write Access Option.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enabling Flash Write Access Option.

Jump to solution
2,528 Views
2winkle
Contributor III

Hi all,

I use MCUXpresso IDE for developing an application to run on iMX RT evaluation board. In the application, I need to write data to the flash. For this, we have to enable write option in the linker script. Is there any way to toggle this option (enable write access) in MCUXpresso IDE without directly meddling with the linker script....?

0 Kudos
Reply
1 Solution
2,353 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Sorry but making modifications to the linker script will provide no ability to write to flash memory.

You need code in your application to write to the external flash. A good starting place would be to take a look at the FlexSPI examples provided as part of the iMX RT1050 SDK.

Regards,

MCUXpresso IDE Support

View solution in original post

1 Reply
2,354 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Sorry but making modifications to the linker script will provide no ability to write to flash memory.

You need code in your application to write to the external flash. A good starting place would be to take a look at the FlexSPI examples provided as part of the iMX RT1050 SDK.

Regards,

MCUXpresso IDE Support