Debugging multiple executables

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debugging multiple executables

2,199 次查看
scottm
Senior Contributor II

Just upgraded to MCUX 10.3.0.  Looks like some nice improvements but I've hit a snag and I'm not sure if it's related to the update or not.

I'm troubleshooting a bootloader problem and I need to be able to step through from my application code to the bootloader, but I'm not getting any source or symbols for the bootloader - which is a separate project with its own ELF output that's loaded on the target with a P&E Cyclone.

In CodeWarrior I can just select the ELF file as an additional executable to debug and it works great.  I'd swear I had this working before in MCUX, and I've tried using the instructions here, but nothing changes - the gdb command doesn't give an error, it just doesn't seem to have any effect.

I had to delete my existing launch configurations from the project when I imported the project into the new MCUX workspace.  Tomorrow I can try recovering them from backups (they might be in version control, too) and going back to the old version, but if someone can tell me how this is supposed to work, I would be most grateful.

With regards to Erich's gdb example in the link given above, I'm not clear what's going on with the offset and why gdb needs to be given one.  The offset is the offset within the ELF file of a particular section, right?  And in his example .text starts at 0x8200.  Shouldn't that be the actual .text contents?  I'd have expected the debug info to be in the .debug_* sections.  And if add-symbol-file always takes an ELF file as input and always needs the offset of .text, why can't it parse the ELF file itself to find the proper section?

In any case, using the same procedure with my executables doesn't give the desired result.

Thanks,

Scott

标签 (1)
0 项奖励
回复
3 回复数

2,071 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI Scott

What's your chip part number?

Jennie Zhang

0 项奖励
回复

2,071 次查看
scottm
Senior Contributor II

I figured it out.  I had two problems - I was misinterpreting Erich's instructions because he referred to the offset of the .text section, but what gdb needs is the load address of .text.  In his example both values were the same.

My next problem was that the ELF file I was trying to load apparently had the symbol information stripped.  Fixed that and I'm able to see my bootloader code now.

Thanks,

Scott

0 项奖励
回复

2,071 次查看
scottm
Senior Contributor II

In this case it's a MK22DX256.  Other projects use the MK22FN1M0 or an MK02 series part.  Same question for those - I just need to load symbols for an extra executable for debugging purposes.

0 项奖励
回复