Build Server - Mcuxpressoidec: Java was started but returned exit code=1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build Server - Mcuxpressoidec: Java was started but returned exit code=1

Jump to solution
6,358 Views
elijah
Contributor III

I am setting up a build server for an MCUXpresso Project, and I have configured it to build the Release configuration. The build finishes correctly but the build server is reporting that it failed with the following message:

 

 

Mcuxpressoidec:
Java was started but returned exit code=1
-Djava.class.path=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\\plugins/org.eclipse.equinox.launcher_1.5.600.v20191014-2022.jar
-os win32
-ws win32
-arch x86_64
-launcher C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\mcuxpressoidec.exe
-name Mcuxpressoidec
--launcher.library C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\\plugins/org.eclipse.equinox.launcher.win32.win32.x86_64_1.1.1100.v20190907-0426\eclipse_1902.dll
-startup C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\\plugins/org.eclipse.equinox.launcher_1.5.600.v20191014-2022.jar
--launcher.overrideVmargs
-application org.eclipse.cdt.managedbuilder.core.headlessbuild
-import ./ProjectName
-cleanBuild ProjectName/Release
-vm C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\jre\bin\server\jvm.dll
-vmargs
-Djava.class.path=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\\plugins/org.eclipse.equinox.launcher_1.5.600.v20191014-2022.jar 
##[error]Process completed with exit code 1.

 

 

I am using a batch file to run the build with the following contents:

 

 

rem Batch file that builds firmware for release

@echo off

rem path to build tools
SET TOOLCHAIN_PATH=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\tools\bin

rem path to command line executable for MCUXpresso
SET IDE=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\mcuxpressoidec.exe

ECHO Extending PATH if not already present
ECHO %PATH%|findstr /i /c:"%TOOLCHAIN_PATH:"=%">nul || set PATH=%PATH%;%TOOLCHAIN_PATH%

ECHO Launching MCUXpresso IDE
"%IDE%" -nosplash --launcher.suppressErrors -application org.eclipse.cdt.managedbuilder.core.headlessbuild -import "./ProjectName" -cleanBuild ProjectName/Release

 

 

Manually running the batch file reports build succeeded with no errors, but the server reports it failed due to the Java error in mcuxpressoidec.exe.

How can I fix this issue?

0 Kudos
Reply
1 Solution
6,099 Views
elijah
Contributor III

I did fix it, I think I had to specify a workspace in the arguments when launching mcuxpressoidec.exe using -data "C:\MCUXpressoIDE_11.2.0_4120\workspace". My batch file is now:

 

rem Batch file that builds firmware for release

@echo off

rem path to build tools
SET TOOLCHAIN_PATH=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\tools\bin

rem path to command line executable for MCUXpresso
SET IDE=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\mcuxpressoidec.exe

ECHO Extending PATH if not already present
ECHO %PATH%|findstr /i /c:"%TOOLCHAIN_PATH:"=%">nul || set PATH=%PATH%;%TOOLCHAIN_PATH%

ECHO Launching MCUXpresso IDE
"%IDE%" -nosplash --launcher.suppressErrors  -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "C:\MCUXpressoIDE_11.2.0_4120\workspace" -import "./ProjName" -cleanBuild ProjName/Release

 


Useful link with a batch file that I played spot the difference with:
https://mcuoneclipse.com/2017/08/03/building-eclipse-and-mcuxpresso-ide-projects-from-the-command-li...

 

View solution in original post

0 Kudos
Reply
6 Replies
6,123 Views
Smatt
Contributor I

I am encountering the same error. The build process itself is successful and reports 0 errors. Also a functional image is generated. 

However, eclipse exits with return code 1, which leads to the build automation system to register the build as failed. 

Could you solve the issue?

0 Kudos
Reply
6,092 Views
elijah
Contributor III

I did fix it, I had to specify a workspace in the arguments when launching mcuxpressoidec.exe using -data "C:\MCUXpressoIDE_11.2.0_4120\workspace". My batch file is now:

rem Batch file that builds firmware for release

@echo off

rem path to build tools
SET TOOLCHAIN_PATH=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\tools\bin

rem path to command line executable for MCUXpresso
SET IDE=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\mcuxpressoidec.exe

ECHO Extending PATH if not already present
ECHO %PATH%|findstr /i /c:"%TOOLCHAIN_PATH:"=%">nul || set PATH=%PATH%;%TOOLCHAIN_PATH%

ECHO Launching MCUXpresso IDE
"%IDE%" -nosplash --launcher.suppressErrors  -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "C:\MCUXpressoIDE_11.2.0_4120\workspace" -import "./ProjectName" -cleanBuild ProjectName/Release

Useful link that has a batch file that I played spot the difference with to find the issue:

https://mcuoneclipse.com/2017/08/03/building-eclipse-and-mcuxpresso-ide-projects-from-the-command-li...

0 Kudos
Reply
6,100 Views
elijah
Contributor III

I did fix it, I think I had to specify a workspace in the arguments when launching mcuxpressoidec.exe using -data "C:\MCUXpressoIDE_11.2.0_4120\workspace". My batch file is now:

 

rem Batch file that builds firmware for release

@echo off

rem path to build tools
SET TOOLCHAIN_PATH=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\tools\bin

rem path to command line executable for MCUXpresso
SET IDE=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\mcuxpressoidec.exe

ECHO Extending PATH if not already present
ECHO %PATH%|findstr /i /c:"%TOOLCHAIN_PATH:"=%">nul || set PATH=%PATH%;%TOOLCHAIN_PATH%

ECHO Launching MCUXpresso IDE
"%IDE%" -nosplash --launcher.suppressErrors  -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "C:\MCUXpressoIDE_11.2.0_4120\workspace" -import "./ProjName" -cleanBuild ProjName/Release

 


Useful link with a batch file that I played spot the difference with:
https://mcuoneclipse.com/2017/08/03/building-eclipse-and-mcuxpresso-ide-projects-from-the-command-li...

 

0 Kudos
Reply
6,090 Views
elijah
Contributor III

https://mcuoneclipse.com/2017/08/03/building-eclipse-and-mcuxpresso-ide-projects-from-the-command-li...

I spotted a difference between the example here and my batch file, which was specifying a workspace.

0 Kudos
Reply
6,351 Views
converse
Senior Contributor V

I would guess that there *is* an error being reported in the build - check the complete build log.

0 Kudos
Reply
6,336 Views
elijah
Contributor III

I've checked through the whole log, the only error is the one in my post which appears at the end after the build finishes

0 Kudos
Reply