Broken Text search

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Broken Text search

8,640件の閲覧回数
cgarcia1
Contributor III

Hi everyone!

I have MCUXpresso IDE v11.10.0 running on Linux, and everything was working right when suddenly search all over the files broke.

The functionality is accessible from "Search" menu and "File..." submenu. This dialog appears:

cgarcia1_0-1726809020025.png

When I click "Search", instead of doing the search and listing the results in the "Search" view, I find this error:

cgarcia1_1-1726809080481.png

Text Search
An internal error occurred during: "File Search Worker".
'byte[] org.eclipse.core.resources.IFile.readNBytes(int)'
An internal error occurred during: "File Search Worker".
'byte[] org.eclipse.core.resources.IFile.readNBytes(int)'
An internal error occurred during: "File Search Worker".
'byte[] org.eclipse.core.resources.IFile.readNBytes(int)'

I read somewhere else that might be related to Copilot4Eclipse plugin, which I also have installed.

The question is: is there any way of properly installing this plugin to avoid breaking this functionality? The rest of the IDE is working great, as before; I can build, I can debug, etc, and also the Copilot4Eclipse is working perfectly fine.

0 件の賞賛
返信
5 返答(返信)

7,445件の閲覧回数
wayne-copilot4eclipse
Contributor I

Hi All,

Big apologies for the recent issue re: Copilot4Eclipse and broken Eclipse search functionality. We have published details on the issue and released Copilot4Eclipse v1.2.2 which resolves the issue. Learn more here: https://github.com/Genuitec/Copilot4Eclipse-community/discussions/23

Wayne
Copilot4Eclipse Team 

0 件の賞賛
返信

8,622件の閲覧回数
ErichStyger
Specialist I

This indeed is very likely a problem of Copilot4Eclipse, so what if you uninstall that plugin or report the issue to the plugin owner?

0 件の賞賛
返信

8,619件の閲覧回数
cgarcia1
Contributor III

After uninstalling the plugin the problem remains. The only way to recover the search functionality is reinstalling MCUXpresso and not installing Copilot4Eclipse again.

My question was more focused on if there's a way, a proper way, of installing this plugin that may not break this feature.

The thing is, for installing this plugin from the Marketplace you cannot do that straight away, as there are some dependences not resolved in MCUXpresso and you need to do some "hacks" to be able to run this plugin in MCUXpresso (not necessary in a normal Eclipse). In fact, I followed the solution posted here (https://www.genuitec.com/forums/topic/cant-install-darkestdark-theme-under-neon-2-nxp-mcuxpress/), but just using another update site: http://download.eclipse.org/releases/2023-06/. I'm a bit suspicious of that "hack", and then I asked if there's a better way of installing this plugin that may avoid this strange issue.

0 件の賞賛
返信

8,401件の閲覧回数
ErichStyger
Specialist I

Looking at the steps or hacks to get the plugin installed, I'm not surprised that it might break things. 'DarkestDark' is infamous to me to break Eclipse basic functionalities.

Having said that, I think it would be better to see with the next MCUXpresso IDE update (new updates align with newer Eclipse), and this might get it solved.

Another option I see is using VS Code for such kind of features where Microsoft has started adding such functionalities directly.

I hope this helps,

Erich

0 件の賞賛
返信

8,602件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @cgarcia1 

So if you don't install this plugin Copilot4Eclipse, this problem won't occur?

BR

Hang

0 件の賞賛
返信