Bootloader for K22FN256

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootloader for K22FN256

1,726件の閲覧回数
mpazzi
Contributor III

Hello,

I have installed MCUXpresso 10.2.1 and downloaded SDK packet with mcu-boot item added.

But on my board I have MK22FN256 and not mcu MK22FN512 how is the only selectable from the SDK packet.

So, how I can modify the bootloader for the correct mcu ? Is it possible ?

Thanks for your support.

Marco

2 返答(返信)

1,530件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Marco,

Since the only difference is the memory size you can just modify the Flash size in the memory
configuration editor to match the MCU you are using. 

Project Properties -> C/C++ Build -> MCU settings

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

1,530件の閲覧回数
mpazzi
Contributor III

Hi Carlos,

thanks for your repley.

On first time I have done that you saying, but it could not work correctly (error for missing some define or something else). So, I dezipped SDK module components and I found file for K22FN256 to substitute the K22F512 and I followed the procedure in chapter 9 of Bootloader v2.6.0 Reference Manual.

It has been laborius but at the end it work fine.

Thanks for your help.

Regards

Marco