Available Software Sites

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Available Software Sites

2,722件の閲覧回数
pch255
Contributor I

Recently installed MCUXpresso v11.0.1 [Build 2563] and when I tried to 'Check for Updates' I discovered that the list of 'Available Software Sites' is completely empty!? How can I refresh this list or do I have to find a default list and manually enter the sites?

0 件の賞賛
返信
4 返答(返信)

2,585件の閲覧回数
pch255
Contributor I

I just uninstalled and reinstalled. This fixed the problem.

On first startup, there is a firewall warning. My guess is that there was a problem allowing firewall access that prevented the list.

Anyway... all is well, thanks for the help and suggestions.

Peter

0 件の賞賛
返信

2,585件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

With a fresh installation of the IDE v11.0.1, I see the following update sites.

pastedImage_1.png

Would you please try switching to a clean workspace and check whether this fixes anything? As a last resort, you could also try starting the IDE with '-clean' (add it in mcuxpressoide.ini). It would be helpful to see the .log file from your workspace as well.

Greetings,
MCUXpresso IDE Support

0 件の賞賛
返信

2,585件の閲覧回数
pch255
Contributor I

Thanks for the help... yes, this list on my system is empty.

I'm not sure how to switch to a clean workspace(?)

Also, what is the .log filename of interest?

Peter

0 件の賞賛
返信

2,585件の閲覧回数
ErichStyger
Specialist I

Hi Peter,

The .log file is a text file located in your workspace .metadata folder:

pastedImage_2.png

For a new/clean workspace: switch to a new folder/empty using this menu:

pastedImage_1.png

I hope this helps,

Erich

0 件の賞賛
返信