Additional software debugging for MCUXpresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Additional software debugging for MCUXpresso IDE

4,219 Views
aberger
Senior Contributor I

I am familiar with Keil µVision IDE which provides some nice functionality: 1.) Debug in simulation mode without downloading code to a target, and 2.) a software logic analyzer for observing signal states vs. time (e.g. different GPIO pins) without the need for an oscilloscope.

Does this sort of functionality exist, perhaps through a 3rd party add-on, or would it be possible to add this functionality?

0 Kudos
Reply
3 Replies

3,786 Views
sutter_zhou
NXP Employee
NXP Employee

You can use FreeMASTER, which is basically a virtual oscilloscope, and it may be more powerful than you want. 

0 Kudos
Reply

3,786 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Sorry, MCUXpresso IDE does not support the use of software simulators. It only supports debugging via the use of a debug probe to real hardware.

Regards,

MCUXpresso IDE Support

2,862 Views
GanesanGuru
Contributor IV

What about now? Whether now is there any support added for debugginh without target system/board? Especially for iMX RT1064 Series & KM34 Series MCUs..

Tags (2)
0 Kudos
Reply