11.2 Build Unresponsive

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

11.2 Build Unresponsive

5,660件の閲覧回数
Keith4DSmith
Contributor V

Having just installed version 11.2, the first issue I have encountered is after starting a build the IDE becomes unresponsive for duration of the build.

This doesn't happen all the time, but always occur on the first build after starting the IDE and then frequently.

The build completes successfully, but there is no output to the Console window. All the output that would have scrolled as the build is proceeding is displayed, but the IDE was unresponsive during the build (blue rotating circle at the cursor).

I frequently perform other actions in the IDE during a build. This is annoying.

I am using Windows 10.

0 件の賞賛
返信
7 返答(返信)

5,547件の閲覧回数
Keith4DSmith
Contributor V

I was able to correct this problem by right-click on Project, select Configure 'Unconvert to xText Project'

0 件の賞賛
返信

5,552件の閲覧回数
converse
Senior Contributor V

Have you checked your firewall and/or antivirus software?

Also, suggest you open an activity monitor (Process Explorer from Microsoft is great) to see what is using all of the CPU time.

0 件の賞賛
返信

5,552件の閲覧回数
Keith4DSmith
Contributor V

As stated, MCUXpresso is compiling correctly, but behind a blue rotating circle. The console is not visible, but at the end of the compilation all the compiler messages are present in the console window. I just wasn't able to see the output in real-time and was locked out from doing any other activity during the compilation. I do not believe there is any other activity. It's as if the opening of the console window is blocked by the compilation.

0 件の賞賛
返信

5,552件の閲覧回数
bastian_schick
Contributor IV

What happens if you limit the number of jobs? I think default is -j(all logic cores).

0 件の賞賛
返信

5,552件の閲覧回数
Keith4DSmith
Contributor V

Yes the default -j is all logic cores. I have 12 logic cores. -j12 is seen during the build.

But as stated, this doesn't happen all the time.

Will set -j6 and see what happens.

0 件の賞賛
返信

5,553件の閲覧回数
Keith4DSmith
Contributor V

Changing to -j6 still has the blue rotating circles, but not all the time.

0 件の賞賛
返信

5,553件の閲覧回数
bastian_schick
Contributor IV

I did not notice such, but an overall slow responsiveness of the IDE. For example opening a folder in the project explorer.

And I have 16 (logical) cores for it.

0 件の賞賛
返信