making a cast from void pointer to pointer to struct results in hardware fault

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

making a cast from void pointer to pointer to struct results in hardware fault

跳至解决方案
3,708 次查看
richardmensah
Contributor II

I am writing a simple blinking LED program in MCUXpresso with ksdk 2.4 and Amazon Freertos.  I intended to create two instances of the same thread definition by passing a void pointer to my structure which contains the GPIO type and pin number to the thread  and later typecast the void pointer to pointer to my structure. however, during debugging, i realised that the new pointer points to a completely different address from my struct data and it always causes a hardware fault. This is however a code which works very well in Kinetis Design studio. I will appreciate help in understanind this problem.


#include <stdio.h>
#include "board.h"
#include "peripherals.h"
#include "pin_mux.h"
#include "clock_config.h"
#include "MK22F51212.h"
#include "fsl_debug_console.h"


typedef struct BLINKY_param {
    GPIO_Type* GPIO;
    uint8_t Pin_name;
} BLINKY_param_t;

enum PINS {
    PTD2  = 2,                  // LED_A
};

#include "FreeRTOS.h"
#include "task.h"
#include "semphr.h"
#include "timers.h"
#include "queue.h"

void air_blinky(void* blinky_parameters) ;
#define mask(x)             ( uint32_t )( 1U << (x) )

int main(void) {

    CLOCK_EnableClock(kCLOCK_PortD);
    PORT_SetPinMux(PORTD,PTD2,kPORT_MuxAsGpio);

    gpio_pin_config_t config = { kGPIO_DigitalOutput, 0 };
    GPIO_PinInit(GPIOD, PTD2, &config);

    BLINKY_param_t Board_A_blinky = {GPIOD,PTD2};

    if (xTaskCreate(air_blinky, "air_blinky_A", 50, &Board_A_blinky, 2,
    NULL) == errCOULD_NOT_ALLOCATE_REQUIRED_MEMORY)
        exit(-1);

    vTaskStartScheduler();

    while (1) {
    }
    return 0;
}

void air_blinky(void* blinky_parameters) {

    const BLINKY_param_t* LED = (BLINKY_param_t*) blinky_parameters;

    TickType_t Lastwakeuptime = xTaskGetTickCount();
    uint8_t Flash_Time = 100;

    for (;;)
    {
        GPIO_PortToggle(LED->GPIO, mask(LED->Pin_name));              // on
        vTaskDelayUntil(&Lastwakeuptime,((Flash_Time * configTICK_RATE_HZ) / (float) 1000));
        GPIO_PortToggle(GPIOD, mask(PTD2));             // off
        vTaskDelayUntil(&Lastwakeuptime,((Flash_Time * configTICK_RATE_HZ) / (float) 1000));
        GPIO_PortToggle(GPIOD, mask(PTD2));              // on
        vTaskDelayUntil(&Lastwakeuptime,((Flash_Time * configTICK_RATE_HZ) / (float) 1000));
        GPIO_PortToggle(GPIOD, mask(PTD2));            // off

        vTaskDelayUntil(&Lastwakeuptime,((2000 * configTICK_RATE_HZ) / (float) 1000));
    }

}

0 项奖励
回复
1 解答
3,430 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Richard:

Sorry for lost tracking this thread.

It seems your issue  resulted from the second parameter of vTaskDelayUntil, it is a const TickType_t. 

  vTaskDelayUntil(&Lastwakeuptime,((Flash_Time * configTICK_RATE_HZ) / (float) 1000));

I suggest you use macro pdMS_TO_TICKS .

Regards

Daniel

在原帖中查看解决方案

3 回复数
3,430 次查看
richardmensah
Contributor II

Hi, Thanks for responding, Please find attached my project

0 项奖励
回复
3,431 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Richard:

Sorry for lost tracking this thread.

It seems your issue  resulted from the second parameter of vTaskDelayUntil, it is a const TickType_t. 

  vTaskDelayUntil(&Lastwakeuptime,((Flash_Time * configTICK_RATE_HZ) / (float) 1000));

I suggest you use macro pdMS_TO_TICKS .

Regards

Daniel

3,430 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Richard:

Could you please attach your project so I can reproduce your issue on my side?

Regards

Daniel

0 项奖励
回复