link error undefined reference

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

link error undefined reference

2,559 Views
harrykoukoutos
Contributor I

I am using MCUXpresso to build an MK10 project. The startup file, startup_mk10d10.cpp, cannot find functions in other modules, for example interrupt service routines or utilities. The IDE gives , as an example, an undefined reference to `PIT1_DriverIRQHandler' error, although it is defined in an other file and a definition line is included. It links only main(). Clearly I have set something wrong! How should I define routines in other modules? Please note that all other files link properly.

Thank you,

Harry Koukoutos

0 Kudos
Reply
2 Replies

2,358 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Given that the file extension of your startup file is ".cpp", I suspect the issue is C vs C++ linkage. There is some information in the following FAQs (which although originally written for LPCXpresso IDE, still apply to MCUXpresso IDE): 

Interrupt Handlers in C++ applications 

https://community.nxp.com/message/630742 

Regards,

MCUXpresso IDE Support

0 Kudos
Reply

2,358 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Harry Koukoutos,

    I highly recommend you to refer to the nxp official code, it will have the according startup file, and the according project.

   Please download it from this link:

https://mcuxpresso.nxp.com/en/select 

  Select the processors as your K10D100M chip, then generate the MCUXpresso IDE project, and try it again.

  If you still have question about it, please kindly let me know.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply