kw38 debug failure via external jlink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kw38 debug failure via external jlink

Jump to solution
1,646 Views
LISI1
Contributor I

example: SDK_2_6_15_MKW38A512xxx4\boards\frdmkw38\wireless_examples\bluetooth\w_uart\freertos

ide: MCUXpresso IDE v11.9.1_2170

Note: Company's own board

 

error:

J-Link GDB Server reported an error.

please check server console for further details.

ERROR:Cound not connect to target.

 

Could you help me with that, thanks!

 

 

 

0 Kudos
Reply
1 Solution
1,600 Views
Itzel_UV
NXP Employee
NXP Employee

Hello,

I will be helping you in this case,

 

I notice that you have 2 questions with the topic involving the KW38, by any chance are they related? I that case we can give a follow up on this threat KW38 debug via PEmicro - NXP Community.

 

Regards,

Itzel

View solution in original post

0 Kudos
Reply
3 Replies
1,533 Views
LISI1
Contributor I

It's a problem with our board,thank you

0 Kudos
Reply
1,601 Views
Itzel_UV
NXP Employee
NXP Employee

Hello,

I will be helping you in this case,

 

I notice that you have 2 questions with the topic involving the KW38, by any chance are they related? I that case we can give a follow up on this threat KW38 debug via PEmicro - NXP Community.

 

Regards,

Itzel

0 Kudos
Reply
1,605 Views
LISI1
Contributor I
Can you help me with that? Thank you
0 Kudos
Reply