ide update / cofig tool issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ide update / cofig tool issue

4,033件の閲覧回数
swaminathanrath
NXP Employee
NXP Employee

Hi,

I am facing couple of tool issue.

Issue 1:               We could not update the config tool in offline mode.

Issue 2:               When we do “Install new software” please refer the attached document

Issue 3:                When we do “check for updates” please refer the attached document.

Thanks & regards,

Swaminathan.R

0 件の賞賛
返信
3 返答(返信)

3,933件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Swaminathan.R,

1. Issue 1: About update MCUxpresso Config Tool on IDE, it seems we can only use online mode.

2.Issue 2 and Issue3, please delete the update site which error remind :

pastedImage_1.png

use the websites below:

pastedImage_2.png

http://download.eclipse.org/tools/cdt/releases/9.4

http://download.eclipse.org/releases/oxygen/ 

http://mcuxpresso.nxp.com/staticdata/updates/kex_ide_5.0/ 

http://www.nxp.com/lgfiles/updates/Eclipse/mcuxpressoide/v10_3/ 

http://www.pemicro.com/eclipse/updates 

Then check whether it can work well.

Have a great day,
Alice

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------

0 件の賞賛
返信

3,933件の閲覧回数
swaminathanrath
NXP Employee
NXP Employee

Hi Alice Yang,

Receiving the below error

pastedImage_1.png

Thanks & regards,

Swaminathan.R

0 件の賞賛
返信

3,933件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello other customers,

Swaminathan sharing it can work well on MCUXpresso IDE v10.3, if any others meet the same problem,

please also try to use latest version, thanks.

BR

Alice

0 件の賞賛
返信