ftm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
7,723件の閲覧回数
652319403
Contributor II

I have some problems in S32K 146

when I used FTM mode,I used FTM3 mode ,but all the FTM clock source are opend ,then I turn off the extra for FTM and use PE to generate code and save it .

  • The second time I opened the project ,all the FTM clock has been opened again, I don't know why .

  • I hope that kind people can help me

  • thank u
ラベル(1)
1 解決策
7,581件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello,


I was able to reproduce the behavior you mentioned. This is a known issue, it has been already fixed, but with the SDK v3.0.1 release.

Best regards,

Victor.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
7,584件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello,

I wasn't able to reproduce the behavior you mentioned.

What version of the S32DS are you using?

What version of the SDK are you using?

Is this an issue of a single project or all your projects behave like this?

 
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

7,584件の閲覧回数
652319403
Contributor II

HI.

thanks for you answer.

The version of the SDK is 2.0.0 

The version of the S32 DS is S32 Design Studio for Arm® 2018.R1

This is  an issue of a single project just in S32 DS

pastedImage_1.png

 I try to use the SDK for 3.0.0 ,and had met the same question.

pastedImage_1.png

0 件の賞賛
返信
7,582件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello,


I was able to reproduce the behavior you mentioned. This is a known issue, it has been already fixed, but with the SDK v3.0.1 release.

Best regards,

Victor.

0 件の賞賛
返信