Windows 10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows 10

1,502 Views
davidmccracken
Contributor I

I have been using MCUXpresso 10.1.1 on Windows 7 without any problems but I can't get this or version 10.2.1 to run at all on Windows 10. On initial execution of the IDE program, version 10.1.1 stalls on the opening logo screen without indicating what it is doing while version 10.2.1 stalls indicating that it is trying to load com.crt.lpcxpresso.brand. Does this program run on Windows 10?

0 Kudos
Reply
1 Reply

1,430 Views
davidmccracken
Contributor I

I have solved this myself. The installation program does succeed when executed by by a user with Admin rights even if not run "As Admin" . However, unless the installer is run "As Admin" the IDE program itself must be run "As Admin" to avoid this initial stall.

0 Kudos
Reply