WDOG - Inconsistencies between Reference Manual, Config Tools, and SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WDOG - Inconsistencies between Reference Manual, Config Tools, and SDK

Jump to solution
2,614 Views
stefano-quantic
Contributor III

iMXRT1176 has a WDOG peripheral with a WCR register. Among its bits are the following (according to Reference Manual IMXRT1170RM, Rev. 2, 06/2023):
WDZST: Watchdog Low Power [...]
0 - Continue timer operation (Default).
1 - Suspend the watchdog timer.
WDBG: Watchdog DEBUG Enable. [...]
0 - Continue WDOG timer operation (Default).
1 - Suspend the watchdog timer.
WDW: Watchdog Disable for Wait. [...]
0 - Continue WDOG timer operation (Default).
1 - Suspend WDOG timer operation.

So, these bit are "set to 1 to freeze the WDOG counter", which is in line with the "Watchdog Disable for Wait" description, but it's the opposite of what "Watchdog DEBUG Enable" suggests.
In "Config Tools | Peripherals | Peripheral drivers (Device specific) | WDOG | Watchdog configuration | Work mode", these bits are described as:
Enabled in wait mode
Enabled in stop mode
Enabled in debug mode

Which again is exactly the opposite of what they are supposed to do (at least according to the RM).
The SDK has this data structure:
typedef struct _wdog_work_mode
{
bool enableWait; /*!< continue or suspend WDOG in wait mode */
bool enableStop; /*!< continue or suspend WDOG in stop mode */
bool enableDebug; /*!< continue or suspend WDOG in debug mode */
} wdog_work_mode_t;

again suggesting a behavior opposite to that of the RM.

What is the actual intended behavior for those bits? Is it actually "suspend the timer if the bit is 1"? In this case, Config Tools and SDK should be updated to use less confusing names; otherwise, the RM is wrong in its description of the bit values.

The RTWDOG peripheral has similar names, except that the RM seems to indicate an "enable the timer if the bit is 1" behavior, so in this case RM/ConfigTools/SDK seem to be all consistent.
For instance, in the CS register:
DBG: Debug Enable [...]
0 - Watchdog disabled in chip debug mode.
1 - Watchdog enabled in chip debug mode.

Is this the intended behavior for RTWDOG (i.e. the opposite of that of WDOG)?

I'm using:
iMXRT1176 chip
Config Tools integrated in MCUXpresso IDE v11.7.0 [Build 9198] [2023-01-17]
SDK 2.13.1

Tags (1)
0 Kudos
Reply
1 Solution
2,558 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @stefano-quantic,

As you mentioned, Config Tools' Work Mode bits description could create misunderstandings about the real behavior of the WCR register, and we will let the team in charge to know about this. Nonetheless, the behavior of both SDK and ConfigTools corresponds to the one described in the IMXRT1170RM.

Regarding the RTWDOG, as you mentioned, it has sort of an opposite behavior to WDOG in its Control Register.

Finally, just to let you know, there is a new MCUXpresso IDE and SDK version (v11.8.0 and v2.14.0). The issues you noticed are there too, but it might be a good idea to change to the newest version.

Thank you for the feedback.

Kind regards, Raul.

View solution in original post

0 Kudos
Reply
1 Reply
2,559 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @stefano-quantic,

As you mentioned, Config Tools' Work Mode bits description could create misunderstandings about the real behavior of the WCR register, and we will let the team in charge to know about this. Nonetheless, the behavior of both SDK and ConfigTools corresponds to the one described in the IMXRT1170RM.

Regarding the RTWDOG, as you mentioned, it has sort of an opposite behavior to WDOG in its Control Register.

Finally, just to let you know, there is a new MCUXpresso IDE and SDK version (v11.8.0 and v2.14.0). The issues you noticed are there too, but it might be a good idea to change to the newest version.

Thank you for the feedback.

Kind regards, Raul.

0 Kudos
Reply