Using a OM40007 and when debugging cant connect to target (LPC54018)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using a OM40007 and when debugging cant connect to target (LPC54018)

888 次查看
jdwil31401
Contributor I

This is the error I get after clicking debug

 

jdwil31401_0-1625788221038.png

jdwil31401_1-1625788270942.pngjdwil31401_2-1625788311333.png

jdwil31401_3-1625788332357.png

I have no clue what I am doing wrong and have tried using the target reset button and the reset button on the target.

I was able to debug 1 time and when I did that the code was running and I didn't hit f8 yet and configured a pin the updated code without stoping the program, ever since I get this error any recommendations are welcomed.

 

Thank you

标记 (1)
0 项奖励
回复
0 回复数